Listen Only Mode of CAN Controller LPC1759

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Listen Only Mode of CAN Controller LPC1759

4,308 Views
gopaljatiya
Contributor I

Hello,

I am trying to build a silent listener on the CAN Bus. I have configured the CANMOD to "Listen Only Mode".

I keep on getting the BUS Error. When i look at the details of it in CANICR, I can see that it is a "form Error".

Method of testing:

Using a PCAN I m sending a message on the CAN Bus. I have a CAN transeiver between the CAN lines and the LPC pins. I can see the the message is received in the buffer but the receive interrupt is never hit. I have enabled the receive interrupt and also enabled the CAN interrupt on the NVIC.

Can someone please let me know what am i doing wrong here, as i can see data in the buffer but receive interrupt is never getting hit. Is there something which I am missing. I can share more details if required to solve this issue.

0 Kudos
Reply
3 Replies

3,625 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Gopal Jatiya

To form CAN bus you need at least 2 active nodes. Message transmitted from one node must be ACKed by (at least one) another nodes. In listen only mode ACK's aren't send。

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,625 Views
gopaljatiya
Contributor I

Thanks for the reply. I have a follow up question.

So, if there is another node that is active and will ACK the message, will listen mode only work if I just want to receive the message? The purpose of my device is to just listen on the CAN bus and never transmit anything.

So, should I operate in "Listen Only Mode" or "Normal" mode when there are other active nodes on the bus. In the mean while I am trying to make another node on this bus that shall be an active node to confirm the behaviour.

0 Kudos
Reply

3,625 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Gopal Jatiya,

1) if there is another node that is active and will ACK the message, will listen mode only work if I just want to receive the message?

    Yes, I think so, please giving a shot.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply