Link2 software, how to modify hsadc code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Link2 software, how to modify hsadc code?

2,518件の閲覧回数
QM
Contributor II

Hi NXP community,

I am new to programming in C for microcontrollers and would appreciate some advice on how I should modify some existing HSADC code.

I have a project which requires me to,

1. Sample at 40 Msps for small chunks of time (~0.2 ms) using the HSADC on the link2 development board (which has an LPC4370 microcontroller)

2. Process the data using FFT (and eventually adding some windowing and averaging)

3. Send the data to a computer via USB.

I am trying to modify the code shown below, which is the example hsadc code that comes as part of the MCUXpressoIDE. I am in the process of selecting the correct DSP function for the FFT from the CMSIS DSP library but am unsure on how to correctly integrate it into the code below. Any advice on the issues I may face with this method would be greatly appreciated. 

Thanks!

/*

 * @brief High speed ADC example

 *

 * @note

 * Copyright(C) NXP Semiconductors, 2013

 * All rights reserved.

 *

 * @par

 * Software that is described herein is for illustrative purposes only

 * which provides customers with programming information regarding the

 * LPC products.  This software is supplied "AS IS" without any warranties of

 * any kind, and NXP Semiconductors and its licensor disclaim any and

 * all warranties, express or implied, including all implied warranties of

 * merchantability, fitness for a particular purpose and non-infringement of

 * intellectual property rights.  NXP Semiconductors assumes no responsibility

 * or liability for the use of the software, conveys no license or rights under any

 * patent, copyright, mask work right, or any other intellectual property rights in

 * or to any products. NXP Semiconductors reserves the right to make changes

 * in the software without notification. NXP Semiconductors also makes no

 * representation or warranty that such application will be suitable for the

 * specified use without further testing or modification.

 *

 * @par

 * Permission to use, copy, modify, and distribute this software and its

 * documentation is hereby granted, under NXP Semiconductors' and its

 * licensor's relevant copyrights in the software, without fee, provided that it

 * is used in conjunction with NXP Semiconductors microcontrollers.  This

 * copyright, permission, and disclaimer notice must appear in all copies of

 * this code.

 */

 

#include "board.h"

#include <stdio.h>

 

/*****************************************************************************

 * Private types/enumerations/variables

 ****************************************************************************/

 

/* The default example uses DMA. To use the example in an interrutp based

   configuration, enable the following definition. */

#define USE_INTERRUPT_MODE

 

/* HSADC clock rate used for sampling */

#define HSADC_CLOCK_RATE (80 * 1000000)

 

/* Base clock lookup table used for finding best HSADC clock rate. Only the

   base clock sources in this table are used as a possible source for the

   HSASC peripheral clock before being divided. Add or remove sources as

   needed, but an exact frequency may not be available unless it's set up

   on an unused PLL or clock input. */

static const CHIP_CGU_CLKIN_T adcBaseClkSources[] = {

CLKIN_IRC, /* Usually 12MHz */

CLKIN_CLKIN, /* External clock in rate */

CLKIN_CRYSTAL, /* Usually 12MHz */

CLKIN_AUDIOPLL, /* Unknown, will be 0 if not configured */

CLKIN_MAINPLL /* Usually 204MHz, may be too fast to use with a divider */

};

 

/* Periodic sample rate in Hz */

#define SAMPLERATE (5)

 

/*****************************************************************************

 * Public types/enumerations/variables

 ****************************************************************************/

 

/* Last saved ADC sample for each input */

volatile uint32_t lastSample[6];

 

/*****************************************************************************

 * Private functions

 ****************************************************************************/

 

/* Returns a computed clock rate based on input clock and divider

   selection */

static uint32_t getClockRate(int clkIndex, uint32_t maxCGU)

{

uint32_t clkRate;

 

clkRate = Chip_Clock_GetClockInputHz(adcBaseClkSources[clkIndex]);

clkRate = clkRate / maxCGU;

 

return clkRate;

}

 

/* Clock setup function for generating approximate HSADC clock. Trim this

   example function as needed to get the size down in a production system. */

static void setupClock(uint32_t rate)

{

CHIP_CGU_IDIV_T freeDivider, bestDivider;

CHIP_CGU_CLKIN_T divider, mappedCGUDuv, savedClkIn;

uint32_t bestRate, testRate, maxCGU, savedMaxCGU;

uint32_t maxCGUDiv;

int clkIndex;

 

/* The HSADC clock (sample) rate is derived from the HSADC base clock

  divided by the HSADC clock divider (only 1 or 2). The HSADC base

  clock can be selected from a number of internal clock sources such

  as the main PLL1, audio PLL, external crystal rate, IRC, RTC, or a

  CGU divider. Unless a PLL is setup for the exact rate desired, a

  rate close to the target rate may be the closest approximation. */

 

/* Determine if there are any free dividers in the CGU. Assumes an

  unused divider is attached to CLOCKINPUT_PD. Divider A can only

  divide 1-4, B/C/D can divide 1-16, E can divider 1-256. */

freeDivider = CLK_IDIV_A; /* Dividers only */

divider = CLKIN_IDIVA; /* CGU clock input sources */

bestDivider = CLK_IDIV_LAST;

while (freeDivider < CLK_IDIV_LAST) {

CHIP_CGU_CLKIN_T clkIn;

 

/* A CGUI divider that is pulled on input down is free */

clkIn = Chip_Clock_GetDividerSource(freeDivider);

if (clkIn == CLKINPUT_PD) {

/* Save available divider and mapped CGU clock divider source */

bestDivider = freeDivider;

mappedCGUDuv = divider;

}

 

/* Try next divider */

freeDivider++;

divider++;

}

 

/* Determine maximum divider value per CGU divider */

if (bestDivider != CLK_IDIV_LAST) {

if (bestDivider == CLK_IDIV_A) {

maxCGUDiv = 4;

}

else if ((bestDivider >= CLK_IDIV_B) && (bestDivider <= CLK_IDIV_D)) {

maxCGUDiv = 16;

}

else {

maxCGUDiv = 256;

}

}

else {

/* No CGU divider available */

maxCGUDiv = 1;

}

 

/* Using the best available maximum CGU and CCU dividers, attempt to

  find a base clock rate that will get as close as possible to the

  target rate without going over the rate. */

savedMaxCGU = 1;

bestRate = 0xFFFFFFFF;

for (clkIndex = 0; clkIndex < (sizeof(adcBaseClkSources) / sizeof(CHIP_CGU_CLKIN_T)); clkIndex++) {

for (maxCGU = 1; maxCGU <= maxCGUDiv; maxCGU++) {

testRate = getClockRate(clkIndex, maxCGU);

if (rate >= testRate) {

if ((rate - testRate) < (rate - bestRate)) {

bestRate = testRate;

savedClkIn = adcBaseClkSources[clkIndex];

savedMaxCGU = maxCGU;

}

}

}

}

 

/* Now to setup clocks */

if (maxCGUDiv == 1) {

/* CCU divider and base clock only */

/* Select best clock as HSADC base clock */

Chip_Clock_SetBaseClock(CLK_BASE_ADCHS, savedClkIn, true, false);

}

else {

/* CCU divider with base clock routed via a CGU divider */

Chip_Clock_SetDivider(bestDivider, savedClkIn, savedMaxCGU);

Chip_Clock_SetBaseClock(CLK_BASE_ADCHS, mappedCGUDuv, true, false);

}

 

/* Enable ADC clock */

Chip_Clock_EnableOpts(CLK_ADCHS, true, true, 1);

}

 

static void timer_setup(void)

{

/* Enable timer 1 clock and reset it */

Chip_TIMER_Init(LPC_TIMER1);

Chip_RGU_TriggerReset(RGU_TIMER1_RST);

while (Chip_RGU_InReset(RGU_TIMER1_RST)) {}

 

/* Timer setup for match and interrupt at SAMPLERATE */

Chip_TIMER_Reset(LPC_TIMER1);

Chip_TIMER_MatchEnableInt(LPC_TIMER1, 1);

Chip_TIMER_SetMatch(LPC_TIMER1, 1, (Chip_Clock_GetRate(CLK_MX_TIMER1) / SAMPLERATE));

Chip_TIMER_ResetOnMatchEnable(LPC_TIMER1, 1);

Chip_TIMER_Enable(LPC_TIMER1);

 

/* Enable timer interrupt */

NVIC_EnableIRQ(TIMER1_IRQn);

NVIC_ClearPendingIRQ(TIMER1_IRQn);

}

 

/*****************************************************************************

 * Public functions

 ****************************************************************************/

 

/**

 * @brief Handle interrupt from 32-bit timer

 * @return Nothing

 */

void TIMER1_IRQHandler(void)

{

/* Clear timer interrupt */

Chip_TIMER_ClearMatch(LPC_TIMER1, 1);

 

/* Reset descriptor pointer to table 0, descriptor 0 and force SW trigger */

Chip_HSADC_SetActiveDescriptor(LPC_ADCHS, 0, 0);

Chip_HSADC_SWTrigger(LPC_ADCHS);

}

 

/**

 * @brief Handle interrupt for HSADC peripheral

 * @return Nothing

 * @note The HSADC IRQ handler is called SPIFI_ADCHS_IRQHandler() on the

 * M0 cores. For the M4 core, it's called ADCHS_IRQHandler().

 */

void ADCHS_IRQHandler(void)

{

uint32_t sts, data, sample, ch;

static bool on;

int prn_delay = 0;

 

/* Toggle LED on each sample interrupt */

on = !on;

Board_LED_Set(0, on);

 

/* Get threshold interrupt status on group 1 and toggle on any crossing */

sts = Chip_HSADC_GetIntStatus(LPC_ADCHS, 1) & Chip_HSADC_GetEnabledInts(LPC_ADCHS, 1);

if (sts & (HSADC_INT1_THCMP_DCROSS(0) | HSADC_INT1_THCMP_DCROSS(1) |

  HSADC_INT1_THCMP_UCROSS(2) | HSADC_INT1_THCMP_UCROSS(3) |

  HSADC_INT1_THCMP_DCROSS(4) | HSADC_INT1_THCMP_UCROSS(5))) {

Board_LED_Set(1, true);

}

else {

Board_LED_Set(1, false);

}

 

/* Clear threshold interrupts statuses */

Chip_HSADC_ClearIntStatus(LPC_ADCHS, 1, sts);

 

/* Pull data from FIFO */

data = Chip_HSADC_GetFIFO(LPC_ADCHS);

while (!(data & HSADC_FIFO_EMPTY)) {

/* Pull sample data and channel from FIFO data */

sample = HSADC_FIFO_SAMPLE(data);

ch = HSADC_FIFO_CHAN_ID(data);

 

/* We don't really have anythng to do with the data,

  so just save it */

lastSample[ch] = sample;

 

/* Next sample */

data = Chip_HSADC_GetFIFO(LPC_ADCHS);

}

 

/* Get ADC interrupt status on group 0 */

sts = Chip_HSADC_GetIntStatus(LPC_ADCHS, 0) & Chip_HSADC_GetEnabledInts(LPC_ADCHS, 0);

 

/* Set LED 2 (if it exists) on an error */

if (sts & (HSADC_INT0_FIFO_OVERFLOW | HSADC_INT0_DSCR_ERROR)) {

Board_LED_Set(2, true);

}

else {

Board_LED_Set(2, false);

}

 

/* Clear group 0 interrupt statuses */

Chip_HSADC_ClearIntStatus(LPC_ADCHS, 0, sts);

}

 

/**

 * @brief main routine for HSADC example

 * @return Function should not exit

 */

int main(void)

{

uint32_t freqHSADC = 0;

uint32_t stored_last_0 = 0;

 

SystemCoreClockUpdate();

Board_Init();

 

/* Setting up the HSADC clock is more complex than other peripherals.

  The HSADC clock is driven directly from the CGU/CCU and has limited

  source and divider options. Because the HSADC clocking is entirely

  handled outside the HSADC peripheral, example code for setting up

  the CGU/CCU to get a rough HSADC clock rate is included in this

  example. */

setupClock(HSADC_CLOCK_RATE);

 

/* Initialize HSADC */

Chip_HSADC_Init(LPC_ADCHS);

 

/* Show the actual HSADC clock rate */

freqHSADC = Chip_HSADC_GetBaseClockRate(LPC_ADCHS);

DEBUGOUT("HSADC sampling rate = %dKHz\r\n", freqHSADC / 1000);

 

/* Setup FIFO trip points for interrupt/DMA to 8 samples, no packing */

Chip_HSADC_SetupFIFO(LPC_ADCHS, 8, false);

 

/* Software trigger only, 0x90 recovery clocks, add channel IF to FIFO entry */

Chip_HSADC_ConfigureTrigger(LPC_ADCHS, HSADC_CONFIG_TRIGGER_SW,

HSADC_CONFIG_TRIGGER_RISEEXT, HSADC_CONFIG_TRIGGER_NOEXTSYNC,

HSADC_CHANNEL_ID_EN_ADD, 0x90);

 

/* Select both positive and negative DC biasing for input 3 */

//Chip_HSADC_SetACDCBias(LPC_ADCHS, 3, HSADC_CHANNEL_DCBIAS, HSADC_CHANNEL_DCBIAS);

Chip_HSADC_SetACDCBias(LPC_ADCHS, 0, HSADC_CHANNEL_DCBIAS, HSADC_CHANNEL_NODCBIAS);

 

/* Set low A threshold to 10% and high A threshold to 90% */

Chip_HSADC_SetThrLowValue(LPC_ADCHS, 0, ((HSADC_MAX_SAMPLEVAL * 1) / 10));

Chip_HSADC_SetThrHighValue(LPC_ADCHS, 0, ((HSADC_MAX_SAMPLEVAL * 9) / 10));

 

/* Set low B threshold to 40% and high B threshold to 60% */

Chip_HSADC_SetThrLowValue(LPC_ADCHS, 1, ((HSADC_MAX_SAMPLEVAL * 4) / 10));

Chip_HSADC_SetThrHighValue(LPC_ADCHS, 1, ((HSADC_MAX_SAMPLEVAL * 6) / 10));

 

/* Setup data format for 2's complement and update clock settings. This function

  should be called whenever a clock change is made to the HSADC */

Chip_HSADC_SetPowerSpeed(LPC_ADCHS, true);

 

/* Enable HSADC power */

Chip_HSADC_EnablePower(LPC_ADCHS);

 

/* Setup HSADC table 0 descriptors */

/* Descriptor entries are mapped as follows */

/* 0 : mapped to input 0, branch to next descriptor after sample, match time

  is 0x90 clocks for the initial sample (must be greater than or equal to

    recovery clocks for auto power-up), test against threshold A */

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 0, (HSADC_DESC_CH(0) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(0x95) | HSADC_DESC_THRESH_A |

HSADC_DESC_RESET_TIMER));

/* 1 : mapped to input 0, branch to next descriptor after sample, match time

  is 1, test against threshold A */

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 1, (HSADC_DESC_CH(0) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(1) |

HSADC_DESC_THRESH_A | HSADC_DESC_RESET_TIMER));

/* 2-3 : mapped to input 1, branch to next descriptor after sample, match time

  is 1 test against threshold A */

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 2, (HSADC_DESC_CH(1) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(1) |

HSADC_DESC_THRESH_A | HSADC_DESC_RESET_TIMER));

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 3, (HSADC_DESC_CH(1) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(1) |

HSADC_DESC_THRESH_A | HSADC_DESC_RESET_TIMER));

/* 4-5 : mapped to input 2, branch to next descriptor after sample, match time

  is 1 test against threshold A */

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 4, (HSADC_DESC_CH(2) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(1) |

HSADC_DESC_THRESH_A | HSADC_DESC_RESET_TIMER));

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 5, (HSADC_DESC_CH(2) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(1) |

HSADC_DESC_THRESH_A | HSADC_DESC_RESET_TIMER));

/* 6 : mapped to input 3, branch to next descriptor after sample, match time

  is 1 test against threshold A */

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 6, (HSADC_DESC_CH(3) |

HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(1) |

HSADC_DESC_THRESH_A | HSADC_DESC_RESET_TIMER));

/* 7 : mapped to input 4, branch to next descriptor after sample, match time

  is 1, test against threshold B, halt after conversion with interrupt, power

    down after conversion */

Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 7, (HSADC_DESC_CH(4) |

HSADC_DESC_HALT | HSADC_DESC_INT | HSADC_DESC_POWERDOWN |

HSADC_DESC_MATCH(1) | HSADC_DESC_THRESH_B | HSADC_DESC_RESET_TIMER));

 

/* Setup HSADC interrupts on group 0 - FIFO trip (full), FIFO overrun

  error, and descriptor statuses */

Chip_HSADC_EnableInts(LPC_ADCHS, 0, (HSADC_INT0_FIFO_FULL | HSADC_INT0_DSCR_DONE |

HSADC_INT0_FIFO_OVERFLOW | HSADC_INT0_DSCR_ERROR));

 

/* Setup HSADC threshold interrupts on group 1 */

Chip_HSADC_EnableInts(LPC_ADCHS, 1,

  (HSADC_INT1_THCMP_DCROSS(0) | HSADC_INT1_THCMP_DCROSS(1) |/* Inputs 0 and 1 below threshold below range */

  HSADC_INT1_THCMP_UCROSS(2) | HSADC_INT1_THCMP_UCROSS(3) |/* Inputs 2 and 3 above threshold range */

  HSADC_INT1_THCMP_DCROSS(4) | /* Inputs 4 downward threshold crossing detect */

  HSADC_INT1_THCMP_UCROSS(5)));/* Inputs 5 upward threshold crossing detect */

 

/* Enable HSADC interrupts in NVIC */

NVIC_EnableIRQ(ADCHS_IRQn);

 

/* Update descriptor tables - needed after updating any descriptors */

Chip_HSADC_UpdateDescTable(LPC_ADCHS, 0);

 

/* Setup periodic timer to perform software triggering */

timer_setup();

 

/* Sleep while waiting for conversions */

while (1) {

__WFI();

if (lastSample[0] >> 6 != stored_last_0 >> 6) {

DEBUGOUT("ADC VALUE[0]: %08x\r\n", lastSample[0]);

stored_last_0 = lastSample[0];

}

}

 

/* Shutdown HSADC when done */

Chip_HSADC_DeInit(LPC_ADCHS);

}

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,484件の閲覧回数
QM
Contributor II

The above code compiles without error as it is just unmodified example code from the LPC_Open library. The point is I want some advice on modifying it to do what I outlined in the first post. 

I have done some more research and have found the following answers to my above questions (the numbers in this post correspond to the numbers in the first post).

1. The hsadc code I have shown above should work to sample at 40 Msps I just need to modify it to do the following,

2. Implement an FFT function from CMSIS DSP library such as arm_cfft_init_q15. Still unsure which FFT function I need to use. The ADC is sampling at 12-bit so this one may be correct but it probably still needs to prepared in some way going from ADC to this function. 

3. I am going to try to use the usbd_rom_libusb example (again from LPC_Open like the hsadc code in the first post) to transfer the processed FFT data to a computer. This example code needs to be used in combination with the hsadc code. 

I will continue to update this with my progress and anything people can add to help would be very appreciated. 

Thank you, 

Quinn

0 件の賞賛
返信

2,492件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello QM,

Recommend you first compile your project and run it , check whether there is problem,

then you can show the problem to us.

 

Regards,

Alice

0 件の賞賛
返信