Library and ROM Driver Sources

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Library and ROM Driver Sources

1,369件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Wed Jul 23 06:16:42 MST 2014
Hi!

I'm working on a project for the LPC11U14 and was having difficulties using the USB driver. The problems were undocumented (error) return codes of some functions and strange "hard faults". All these had ./lpc_chip_11uxx_lib/libs/libusbd_11uxx_lib.a in the call stack.

Usually I just look through the sources and find reasons for that behavior. In nearly all cases the problems clearly were caused by some erronous setup or preparation by me, before calling the driver functions.

Unfortunately, there is no source code, which forced me to the tedious, frustrating and time consuming "try and error" approach.

Could you please provide the sources of the above mentioned library?

Thinking further, every developer using the newer devices with integrated ROM drivers has the exact same problem, that he can't find out the true reasons for buggy behavior. Therefore I also ask to provide the ROM driver source code. The best solution would be to have all the various revisions available so one can use the exact same sources as used for the current silicon revision at hand. Even better would be added debug and symbol information (e.g. included in the ELF files), so your customers can debug the ROM drivers and see how their own code is interacting with it.

Thanks
  Hansi
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,321件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Tue Nov 25 03:13:42 MST 2014
Hi!

Any news on this issue?

Thanks
  Hansi
0 件の賞賛
返信

1,321件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Belias on Wed Jul 23 07:20:08 MST 2014
I would also strongly appreciate this! While working with the ROM drivers it is often hard enough to find out which driver is causing the problem (I had the I2C and UART drivers sticking in loops in the ROM driver, for an unknown reason). Then you have to get the address from the call stack, look into the datasheet which driver this address might  belong to.

Debug symbols would make this easy going!
0 件の賞賛
返信