Level triggering not working on LPC 804 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Level triggering not working on LPC 804 board

ソリューションへジャンプ
3,259件の閲覧回数
Balaji_KG
Contributor II

Hi,

       Currently I am working on LPC804 controller. In that pin interrupt method only working in EDGE triggering. Level triggering method isn't working. I tried the LPCOpen demo code also. Kindly give some reference on this.

タグ(1)
0 件の賞賛
返信
1 解決策
3,203件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Balaji_KG 

 

I tested your project with lpcxpresso804 board, the PINT with High level interrupt  works well.

You can set a breakpoint in PIN_INT0 interrupt function as below:

Alice_Yang_0-1687245659132.png

 

When input high level on pio0_13 pin, will enter this interrupt function.

 

BR

Alice

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,212件の閲覧回数
Balaji_KG
Contributor II

Hello @Alice_Yang ,

 I attached my project for your reference.

0 件の賞賛
返信
3,204件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Balaji_KG 

 

I tested your project with lpcxpresso804 board, the PINT with High level interrupt  works well.

You can set a breakpoint in PIN_INT0 interrupt function as below:

Alice_Yang_0-1687245659132.png

 

When input high level on pio0_13 pin, will enter this interrupt function.

 

BR

Alice

 

0 件の賞賛
返信
3,196件の閲覧回数
Balaji_KG
Contributor II

Dear @Alice_Yang ,

                    I will check this on my board. Thanks for your support.

0 件の賞賛
返信
3,231件の閲覧回数
Balaji_KG
Contributor II

Dear @Alice_Yang ,

                         I checked the demo code through MCU expresso IDE. In that I configured GPIO pin and all registers properly. still, Level triggering not working but edge triggering is working properly. 

0 件の賞賛
返信
3,220件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Balaji_KG 

Please share your project, thanks.

 

BR

Alice

0 件の賞賛
返信
3,237件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Balaji_KG 

How do you test on LPCopen demo? How about change to another pin?

And please check all the related registers configured correctlly.

 

BR

Alice

0 件の賞賛
返信