Led indicator to Reset button

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Led indicator to Reset button

1,746 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Mon Feb 08 03:03:18 MST 2016
Hello!,

In LPC1549 Expresso board schematic in page 3, label RESET there is a Led Osram  LS Q976 with 2.2KΩ resistor.

http://www.osram-os.com/Graphics/XPic9/00128792_0.pdf

Ohm law say:

R = V / I

R = (3.3 - 2) / 0,025A = 52Ω   0.032 watts

Why the designer chose 2.2KΩ?.  I must be missing something.

Regards
标签 (1)
0 项奖励
回复
2 回复数

1,714 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Sun Apr 24 08:02:13 MST 2016
Thanks Ian,

Regards
0 项奖励
回复

1,714 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sun Mar 27 09:06:34 MST 2016
because he didn't want it full brightness.
0 项奖励
回复