Led indicator to Reset button

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Led indicator to Reset button

1,720件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Mon Feb 08 03:03:18 MST 2016
Hello!,

In LPC1549 Expresso board schematic in page 3, label RESET there is a Led Osram  LS Q976 with 2.2KΩ resistor.

http://www.osram-os.com/Graphics/XPic9/00128792_0.pdf

Ohm law say:

R = V / I

R = (3.3 - 2) / 0,025A = 52Ω   0.032 watts

Why the designer chose 2.2KΩ?.  I must be missing something.

Regards
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,688件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Sun Apr 24 08:02:13 MST 2016
Thanks Ian,

Regards
0 件の賞賛
返信

1,688件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sun Mar 27 09:06:34 MST 2016
because he didn't want it full brightness.
0 件の賞賛
返信