LX2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2080

2,122 Views
YY2410
Contributor III

The LX2080 automotive-grade chip fails to start at a low temperature of -35°C, with no serial port output and inability to enter Hard-code mode. Measurements indicate that the power supply, clock, and reset signals are all normal. What could be the possible reason?#LX2080CA72232B

Tags (2)
0 Kudos
Reply
3 Replies

2,044 Views
June_Lu
NXP TechSupport
NXP TechSupport

How do you identify the Power-up sequence is fine?

If you could boot in the room temperature, you don't configure anything.

You could input your question in Chinese.

0 Kudos
Reply

2,091 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please check the signals of the LX2160A Reference Manual, page 138, 4.9.6 Power-On Reset Sequence Timing.

And then check the signals status per the stage of 4.9.5 Power-On Reset Sequence Detailed Description to check which stage is wrong.

Thanks

0 Kudos
Reply

2,072 Views
YY2410
Contributor III

Power-up sequence is fine, signals status is not convenient for measurement; and there is one more question,Refer to the attached picture,I am using an automotive-grade chip. Do I need to configure anything in the hardware or software?

0 Kudos
Reply