LWIP in Eclipse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP in Eclipse

1,915 Views
vishakhadakhane
Contributor III

Hello , I am new to eclipse and i am done with GPIO toggling . Now I would like to run Ethernet with LWIP .I don't know from where to start with. Is there a sample example for Ethernet  available in eclipse?  i am working on LPC1769 controller.Thank you!

Best regards,

Vishakha

0 Kudos
Reply
1 Reply

1,786 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Vishakha,

There are two examples in the LPCOpen folder within the MCUXpresso IDE.

Both are examples containing lwip one uses Free-RTOS and the other is a stand alone example(without an RTOS).

MCUXpresso is an eclipse-based IDE. You download it from here.  

Once downloaded you can follow this path in your computer to find the LPCOpen folder which contains many examples from different microcontrollers, including the LPC1769.

C:\nxp\MCUXpressoIDE_11.0.0_2516\ide\Examples\LPCOpen

Inside the folder you will find several examples using different peripherals. However the two that may interest you are named:

lwip_tcpecho_freertos

lwip_tcpecho_sa

Let me know if you have any questions.

Best Regards,

Sabina

0 Kudos
Reply