LTC2335-16 reference code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTC2335-16 reference code

Jump to solution
7,118 Views
nithin3200
Contributor IV

Hello 

I need to interface LTC2335-16 adc with LPCXpresso54628.For that is there any sample code is available. if not, then how I can interface?

 

 

Labels (1)
0 Kudos
Reply
1 Solution
6,901 Views
nithin3200
Contributor IV

Hi,

 

Thanks for the replay. Am sharing the spi pins for two adc(SDI,SDO,SCLK,CNV) chip select 1&2 and busy1&2 pins are given separately .

View solution in original post

0 Kudos
Reply
11 Replies
7,066 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have downloaded the data sheet of LTC2335-16 Linear website.

Because you want to interface with LPC54628, this is my suggestion. The LPC54628 has SCTimer, PINT and SPI module, I think you can connect the LPC54628 with LTC2335-16 in this way:

1)you can use SCTimer to generate PWM signal and output it to SCTimer_OUTx and connect the SCTimer_OUTx to CNV pin of LTC2335-16 .

2)Connect the Busy signal of LTC2335-16 to any GPIO pin of LPC54628, configure the GPIO pin as PINT0 triggering source, when the Busy signal is low, an PINT0 interrupt is triggered, the PINT0_ISR() function is executed.

3)connect one SPI module of LPC54628 as master to LTC2335-16, in detail

master SPI module of LPC54628        LTC2335-16

/CS                                                      /CS

SCK                                                    SCKI

MOSI                                                  SDI

MISO                                                  SDO

From software, you can write the SPI transmitter data register in PINT0_ISR()  to   launch the SPI timing, you can use SPI polling mode to get the ADC result

The PWM signal is used to control the ADC conversion rate

Hope it can help you

BR

XiangJun Rong

 

7,060 Views
nithin3200
Contributor IV

Hi,

 

Can you share the LPC54628 has SCTimer sample code. So i will have the better idea.

 

 

BR

Nithin

0 Kudos
Reply
7,055 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls download SDK package of LPC54628 from the website:

https://mcuxpresso.nxp.com/en/welcome

There is PWM generation example and SPI master example in the SDK package

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply
7,049 Views
nithin3200
Contributor IV

Hi,

 

Thanks for the reply.

My design am using two LTC2335 adc and need to read every one millisecond this both adc and push data to a buffer.so how i switch this two adc ?

To send data to adc need to use control word so that i need to write PINTO_ISR() function one by one for two adc .and read data I need decode the data from polling method one by one. is that right?. if am wrong please tell me how to handle this two adc read write operation I millisecond.

your reference am sharing cnv pin. Sck 1khz, SC Timer pwm setting 1 khz.

 

BR 

Nithin

0 Kudos
Reply
6,985 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC54628 has multiple SPI modules, multiple Pint modules and the same SCTimer can output multiple PWM signals with the same PWM signal frequency.

You can connect like:

ADC0: one PWM  output signal from SCTimer as ADC conversion signal, the ADC0 Busy signal triggers for example PINT0 module, use SPI3 to transfer spi data.

 

ADC1: another PWM  output signal from SCTimer as ADC1 conversion signal, the ADC1 Busy signal triggers for example PINT1 module, use SPI4 to transfer spi data.

In this way, both the ADC0 and ADC1 work independently.

 

Hope it is helpful

BR

XiangJun Rong

 

6,973 Views
nithin3200
Contributor IV

Hi,

 

Can you show me one example for ADC0: one PWM  output signal from SCTimer as ADC conversion signal, the ADC0 Busy signal triggers for example PINT0 module, use SPI3 to transfer spi data.

0 Kudos
Reply
6,962 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that all the SCTimer, PINTx and SPI all have the example, you have to assemble them in one project, and develop the code yourself

BR

XiangJun Rong

0 Kudos
Reply
6,954 Views
nithin3200
Contributor IV

Hi,

 

lpcxpresso54618_sctimer_simple_pwm :- SCTimer

lpcxpresso54618_pint_pin_interrupt      :-PINTx 

lpcxpresso54608_spi_interrupt :-SPI 

Can I use this example for my project.

0 Kudos
Reply
6,932 Views
nithin3200
Contributor IV

Hi ,

 

For your reference am using same spi for both adc

0 Kudos
Reply
6,911 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you have to use two SPI modules, each ADC requires one SPI module.

BR

XiangJun Rong

6,902 Views
nithin3200
Contributor IV

Hi,

 

Thanks for the replay. Am sharing the spi pins for two adc(SDI,SDO,SCLK,CNV) chip select 1&2 and busy1&2 pins are given separately .

0 Kudos
Reply