LPCxxx 2 Drone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCxxx 2 Drone

1,838件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Sat Nov 21 02:47:26 MST 2015
Hello,

I decided to use NXP for my next project. A autopilot to planner, rovers and multi-copters. With open-source license.

But I have some doubts.

At first I had thought to use a LPC1769 + LPC2141 as explained in AN10898, + other Cortex-m0+ to Bosch Sensors.

But now I have seen the LPC54102 integrating a Cortex-M4 and Cortex-M0 and seems to be improved drones but can not find the LQFP64 package. In this reference it is only DigiKey LPC54102J512UK49Z and it has a package 49-WLCSP (Ball Grid Array).

Also I need to know if there is a library and the module (footprint in LQFP) of LPC54102 for Kicad.  Because it would have to create them manually. In both cases I need to know if the LQFP64 package will be available in production.

In this web page say that FreeRTOS+CLI and FreeRTOS+FAT are for free commercial licenses to users of LPC17xx and LPC18xx microcontrollers, it's also applicable to LPC54102 ?

http://www.freertos.org/FreeRTOS-Plus/BSP_Solutions/NXP/index.html


Quote:
Note that users of LPC17xx and LPC18xx microcontrollers also qualify for free commercial licenses for FreeRTOS+CLI and FreeRTOS+FAT SL. Also see the FreeRTOS page on NXP's LPCWare website.




Best regards,
Javier
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,713件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Sat Nov 21 10:50:41 MST 2015



Quote:
At first I had thought to use a LPC1769 + LPC2141 as explained in AN10898, + other Cortex-m0+ to Bosch Sensors.

But now I have seen the LPC54102 integrating a Cortex-M4 and Cortex-M0 and seems to be improved drones



Sorry but my baby wakes up when I'm writing. I wanted to ask you recommend, if using an LPC 54102 or use a LPC1769 and a Cortex-m0+

Best regards
0 件の賞賛
返信

1,713件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Sat Nov 21 08:12:38 MST 2015
Sorry R2D2 but I do not know the meaning of 'Qualification' in english for this context. I speak spanish and I understand some English.

¿Qualification means that the reference will be in production soon?

Thanks
0 件の賞賛
返信

1,713件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Nov 21 04:17:16 MST 2015
:quest:

Google:

LPC54102


NXP Search

shows Product status = [color=#f00]Qualification[/color]...
0 件の賞賛
返信