LPCpresso43S67: No compatible emulator available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCpresso43S67: No compatible emulator available

1,982件の閲覧回数
ZJane
Contributor I

The board make DFU link and J5 USB connector.

No device were found in the device manager , and cannot be detected in debugger.

system: win11;  development board:LPC43S67

1.png20230614202031.jpg

0 件の賞賛
返信
3 返答(返信)

1,953件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I review your case I do not if your problem is the debugger on the board or win11, the issues with win11 are not a priority.

Try with HOST DEVICE DRIVERS

Pavel_Hernandez_0-1686775405696.png

LPCXpresso43S67 Development Board | NXP Semiconductors

Try too update the debugger on the board with J-link.

LPCScrypt v2.1.2 | NXP Semiconductors

LPC-Link2 Debug Probe Firmware Programming (nxp.com)

Best regards,
Pavel

0 件の賞賛
返信

1,929件の閲覧回数
ZJane
Contributor I

I installed the host driver and update the Jlink driver.

file1:  lpc_driver_setup.exe

file2: JLink_Windows_V788g_i386.exe

It doesn't work. 

0 件の賞賛
返信

1,914件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, could you update the firmware of your debugger on the board?

LPCScrypt v2.1.2 | NXP Semiconductors

Pavel_Hernandez_0-1686861349990.png

You will need to put the board in DFU mode Device Firmware Update.

Pavel_Hernandez_1-1686861415857.png

Best regards,
Pavel

0 件の賞賛
返信