LPCopen for LPCXpresso4337/4367?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCopen for LPCXpresso4337/4367?

1,137件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by a.papanikolaou on Fri May 20 02:58:59 MST 2016
Hello,

the link to download LPCOpen v2.16 for the LPCXpresso4337 boards on the NXP site is broken. Is this due to the migration between websites or is this library currently unavailable? And unfortunately there seems to be no earlier versions of LPCOpen for this board. Furthermore, links to the lib for other IDEs seem to be working fine...
I am working on a project with tight deadlines and recently purchased the LPCXpresso4367 board to start experimentation. Will there be a quick fix or should I be looking at alternative boards/IDEs?

Thank you
Antonis
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,096件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,096件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 8473 on Fri May 20 05:57:26 MST 2016
Hello Antonis,

the LPCXpresso-installation should include a copy, e.g.:

C:\nxp\LPCXpresso_8.1.4_606\lpcxpresso\Examples\LPCOpen


Regards
0 件の賞賛
返信