LPCXpresso824-MAX board - missing schematics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso824-MAX board - missing schematics

3,063件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Mon Oct 27 12:00:58 MST 2014
From http://www.lpcware.com/content/devboard/lpcxpresso-max-developer-boards there is a broken  link to the schematic diagram: http://www.lpcware.com/content/lpcxpresso824-max-schematic.

On the LPCXpresso824-MAX's  "home page" http://www.nxp.com/demoboard/OM13071.html there is no schematic diagram either....
ラベル(1)
0 件の賞賛
返信
8 返答(返信)

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Wed Oct 29 07:41:16 MST 2014

Quote: larsen
I would suggest that the download "All documentation" should contain both the user manual, datasheet and schematics.


...I would like to ask why you don't find this a good idea - Personally I find it attractive to not have to scatter gather relevant information, but have the experts doing this for me.

If there are Revision A boards on the market, then the revision A schematics should be published as well. Mine is Rev B so I am fine, but maybe others aren't.
0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpecosystem on Tue Oct 28 08:55:30 MST 2014
The page with the schematic had been created incorrectly such that those of us inside NXP could see it, but no-one else could. The problem should now be corrected and be visible to you on the LPC800 family downloads and LPCXpresso MAX  boards pages. The direct URL is:
http://www.lpcware.com/content/nxpfile/lpcxpresso824-max-schematic

Looks like capiman was very good with his timing to re-check (thanks capiman  :) )

We apologize for the inconvenience.
0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Tue Oct 28 08:49:13 MST 2014
Original (from above):
http://www.lpcware.com/content/lpcxpresso824-max-schematic
This works (from other thread):
http://www.lpcware.com/content/nxpfile/lpcxpresso824-max-schematic
0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Tue Oct 28 07:29:56 MST 2014
@Paul
Can you try to logout from lpcware and see, if you can still be able to access the page?
0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Tue Oct 28 07:26:08 MST 2014
All the links work for me, but I will report this to our web team.
Thank you for your feedback.

Paul
0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Tue Oct 28 06:55:36 MST 2014

Quote: NXP_Paul

When I look at the LPCXpresso824-MAX home page http://www.nxp.com/demoboard/OM13071.html, there is a link to the schematics if you scroll to the bottom of the page.



Sorry I cannot find this link to the schematic you refer to. In any case:

I would suggest that the download "All documentation" should contain both the user manual, datasheet and schematics.

Also I can confirm that the link http://www.lpcware.com/content/lpcxpresso824-max-schematic gives this text:
This page is inaccessible. This usually means that you do not have the permissions to view the content on this page. Site content may be disabled for a number of different reasons, such as updates, replacement by new content, or limited access. If you feel you've reached this page in error, or that the content of this page, please leave feedback by clicking the feedback tab.
0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Tue Oct 28 06:09:57 MST 2014
@Paul
I can reproduce the error. When clicking on
http://www.lpcware.com/content/lpcxpresso824-max-schematic
(also in the original message or your previous message, same on given webpage in box "Variants")
it gives a page
"Error - inaccessible page"
"This page is inaccessible."
(German) Firefox 33.0 on Windows (64 bit)
Perhaps the page is not given rights for the public?

0 件の賞賛
返信

2,990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Tue Oct 28 05:57:50 MST 2014
Hello
I cannot confirm your results.  When I click on the LPC824 schematic, it brings me to:
http://www.lpcware.com/content/lpcxpresso824-max-schematic.  Clicking on the link on this page brings me to:
http://www.lpcware.com/system/files/LPC824_Xpresso_v2_schematic_Rev_B.pdf

When I look at the LPCXpresso824-MAX home page http://www.nxp.com/demoboard/OM13071.html, there is a link to the schematics if you scroll to the bottom of the page.

Please let me know if I misunderstood your inquiry.

Regards
Paul
0 件の賞賛
返信