LPCXpresso55S36 I3C SDK examples not working (possible SDA risetime issue)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso55S36 I3C SDK examples not working (possible SDA risetime issue)

3,552 次查看
amonreal
Contributor I

Hi,

I am working on an LPCXpresso 55S36 and using SDKs "lpcxpresso55s36_i3c_polling_b2b_transfer_master" and "lpcxpresso55s36_i3c_master_read_sensor_icm42688p" and I haven't been able to make either of them work properly.
It seems like the SCL line (J9 pin 20) is working properly but I see a really long rise time on the SDA line (J9 pin 18). I have attached an oscilloscope capture for both SDKs

 


Could I have a setup issue, my board be damaged, or have you seen this type of issue before? Does the SDA line require a pullup? Thanks

 

Best,
Antonio 

标签 (1)
0 项奖励
回复
3 回复数

3,532 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @amonreal 

 

Please refer to readme.txt to configure your board:

Alice_Yang_0-1682061110673.png

 

BR

Alice 

0 项奖励
回复

3,521 次查看
amonreal
Contributor I

Hi @Alice_Yang 

Thanks for your reply. I did do all those steps when I got these captures as you can see from the third picture attached on my original post. Do you have any more pointers?

0 项奖励
回复

3,501 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @amonreal 

If run the demo "lpcxpresso55s36_i3c_polling_b2b_transfer_master", need connect with another board as slave. About the demo "lpcxpresso55s36_i3c_master_read_sensor_icm42688p", I tested it before, it can well, no issue, recommend you check carefully again refer to readme.txt.

 

BR

Alice

0 项奖励
回复