LPCXpresso55S16 file system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso55S16 file system

1,047件の閲覧回数
ahmed007
Contributor II

Hi there,

I'm looking for a sample usage of a file system on the on-chip internal flash of the LPCXpresso55S16. I attempted to use FatFs from the SDK, but I couldn't find an example despite downloading FatFs within the SDK. Additionally, I tried using littlefs, but encountered an error during the mounting process. It's possible that I'm using incorrect parameters or making other mistakes, as I only tried a basic example of mounting the file system without success.

I would greatly appreciate any assistance.

Thanks, Ahmed

ラベル(1)
0 件の賞賛
返信
1 返信

1,038件の閲覧回数
ErichStyger
Specialist I
0 件の賞賛
返信