LPCXpresso54628 USB vendor specific example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso54628 USB vendor specific example

3,253件の閲覧回数
vinu_narayanan
Contributor I

Hi , 

Can anybody provide a simple vendor specific USB device example project for LPCXpresso54628 with MCUXpresso  IDE ? a simple USB example to send some data in a bulk end point would do ?I am a USB newbie and am breaking my head for last one week to implement one . There are lot of examples with generic classes but none with a vendor specific one . Documents also seems to be very high lever for newbie like me .

ラベル(1)
  • USB

タグ(1)
4 返答(返信)

3,094件の閲覧回数
vinu_narayanan
Contributor I

Finally after 3 weeks of effort I made it working . 

Thanks for all the support . 

0 件の賞賛
返信

3,094件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Good to know it. You are welcome.

0 件の賞賛
返信

3,094件の閲覧回数
carstengroen
Senior Contributor II

Vinu,

you will probably get lost in the SDK samples, at least I did :smileyhappy:
I ended up doing this: https://community.nxp.com/thread/447669 

Maybe it can be of some help to you

3,094件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi vinu narayanan 

Please download MCUXpresso SDK from this url:

Welcome | MCUXpresso SDK Builder 

Download LPC54628 SDK package. under this folder, there is a set of usb examples. Hope this will help you.

{LPCXpresso54628 SDK folder}\boards\lpcxpresso54628\usb_examples


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------