LPCXpresso54608 for Mine Rescue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso54608 for Mine Rescue

1,002件の閲覧回数
zl001
Contributor I

For these years,we  are always working for Mine rescue and escape equipment.I want to apply the LPC board for the new escape panel with OSIII systerm. I  used   the LPC824 for experiment.

1. Full speed USB ports for the transport order.

2.Ethernet for the big Data communicaiton.

3.Using Temperature sensor ,air pressure sensor,water sensor,O2 and CO sensor for base data and display on the LCD and PC.

4.Using three axis gyroscope sensor and acceleration  sensor for the class gesture and showing data on the LCD.

I hope I can apply the LPCXpresso54608 board and use it to do more worthwhile  work.Thanks.

 

タグ(1)
0 件の賞賛
返信
0 返答(返信)