LPCXpresso1549 board with IAR Embeded Workbench -> Debug Problem Verification error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso1549 board with IAR Embeded Workbench -> Debug Problem Verification error

1,825 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kai.becker on Thu Aug 28 07:30:50 MST 2014
Hi,

I hope this is the right forum to post my question/problem.
I´ve used the search function for the forum and also a google search,
but couldn´t find a usefull tip to solve my problem.

I have bougth an LPCXpresso1549 board and I have the IAR Embedded Workbench 7.20 Standard Edition.
I´ve loaded the example workspace that includes all sample projects.
I chose the periph_blinky projekt and compiled it. Everything went fine.

Then I have tried to debug the project. First the flash action starts.
Then the Workbench reports an error.

When I look at the output window I see the following messages.

Thu Aug 28, 2014 16:02:47: LowLevelReset(software, delay 200)
Thu Aug 28, 2014 16:02:47: LowLevelReset(script, delay 200)
Thu Aug 28, 2014 16:02:47: Calling reset script: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0_2\arm\config\debugger\NXP\LPC15xx.ProbeScript@ResetAndStopAtUser
Thu Aug 28, 2014 16:02:47: No script found.
Thu Aug 28, 2014 16:02:47: Verification error at 0x00000000: mem = 0x00, file = 0x10
Thu Aug 28, 2014 16:02:47: Download completed but verification failed.
Thu Aug 28, 2014 16:02:47: LowLevelReset(software, delay 200)
Thu Aug 28, 2014 16:02:48: Target reset
Thu Aug 28, 2014 16:02:48: There were 1 error and 3 warnings during the initialization of the debugging session.
Thu Aug 28, 2014 16:02:51: Stopped by a vector catch ...

So the problem seems to be the "Verification error".

I have used the "DFUSec.exe (LPC-Link 2 Configuration Tool) tool to download an image to the LPC4322 debugger chip mounted on the  LPCXpresso1549 board.
The only image that downloaded successfully was the "CMSIS-DAP LPCXpresso V2 CMSIS-DAP debugger image"
All other images failed to load.

The verification error persitis after all tries to start a working debugging session.

So my question is, if anyone knows this kind of error, or if anyone has a hint what I could do to solve this problem.

Thanks for every help in advantage

Kai






标签 (1)
0 项奖励
回复
1 回复

1,744 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pradeep salloju on Tue Feb 24 22:22:17 MST 2015
I am also facing same issue with LPCXpresso54102 Evaluation board , could any one help me out of this problem.
0 项奖励
回复