LPCXpresso breakpoints do not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso breakpoints do not work

2,343件の閲覧回数
whatag721
Contributor I

Hello! I am using an LPC1115 board with the latest version of the LPCXpresso IDE. Previously I was running examples and my own code and break points were working fine. Now when I try to add a break point instead of a blue dot I get an blue line with a little arrow. These types of breakpoints never work, they do not stop the code. What kind of breakpoint is this and how do I get back to using regular break points? I cannot find any help in the user manual or the help. The unknown breakpoint type is shown in the picture.

Thanks,

Adam

ラベル(1)
0 件の賞賛
返信
1 返信

2,171件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

I suspect that you have accidentially  selected the "Skip all breakpoints" icon in the Breakpoints view (or on the main toolbar) which will temporarily disable all breakpoints. 

Note that LPCXpresso IDE is no longer being developed/maintained and was replaced by MCUXpresso IDE over a year ago. The current version of MCUXpresso IDE is v10.2.0. For more details visit http://www.nxp.com/mcuxpresso/ide. And if you have questions, post them to the IDE forum at: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide 

Regards,

MCUXpresso IDE Support.