LPCXpresso board LPC812 periph_uart example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso board LPC812 periph_uart example

1,359 次查看
walt_lpc
Contributor I

Hello, I am able to get the  periph_uart example to run, the leds blink, however the board is not outputting anything

on the serial port.

Things done:

Soldered a header into J7, and wired a USB to serial cable (one I have used on a cubieboard)

Confirmed the serial cable is working by tying Tx and Rx together

Black wire from usb cable to board ground

White wire from usb cable to LPC812 PIO0_0, Tx

Green wire from usb cable to LPC812 PIO0_4, Rx

Set the baud rate to 115200 in both Windows device manager, and putty terminal

I have not made any changes to the example project. Project is from LPSOpen.

LPCXpresso v8.2.2 [Build 650] [2016-09-09]

I thought maybe it was not possible to use the board's uart while in debug mode, so I built and tried a release version,

but had the same negative result. Any thoughts would be appreciated. Thanks!

... Two minutes after posting this I swapped Rx and Tx connections and it worked. I had hesitated to try this because

I was sure the wiring was ok, same as on cubieboard, and I was afraid of damaging the board. However, after checking

there pdf schematic, there are are 220 ohm resistors in series with the pins so I went ahead and swapped the wires.

标签 (3)
标记 (1)
0 项奖励
回复
1 回复

1,163 次查看
soledad
NXP Employee
NXP Employee

thank you for your input :smileywink:

Regards

Sol

0 项奖励
回复