LPCXpresso OM13058 LPC11U68 VREFN maximum voltage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso OM13058 LPC11U68 VREFN maximum voltage?

1,355件の閲覧回数
dirtyd
Contributor I

Is there a specification for maximum VREFN voltage? In the datasheet and user manual there are recommendations for best performance, but no hard limits except for the upper limit on VREFP.

From the user manual, page 304 :

"Remark: For best performance, select VREFP and VREFN at the same voltage levels as VDDA and VSSA. When selecting VREFP and VREFN different from VDDA and VSSA , ensure that the voltage midpoints are the same:
(VREFP-VREFN)/2 + VREFN = VDDA/2"

I am attempting to set VREFN at approximately 2.7V and VREFP at approximately 3.2V, for about 0.5V difference, using LM385 voltage references. VREFP pin is fine, I can connect either reference to it, but with VREFN pin it is pulled down to 0.85V. I can't see anything on the OM13058 schematic to explain this so I am wondering if it some kind of internal protection in the MCU itself?

Does anyone have any experience trying to use a similar high VREFN voltage?

ラベル(2)
0 件の賞賛
返信
1 返信

1,190件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

The set of the VREFP and VREFN should follow the rules:

1. The VREFP voltage level must be between 2.4 V and Vdda.

2. (VREFP-VREFN)/2 + VREFN = VDDA/2

Hole it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信