LPCXpresso LPC1769 Emulator Not Found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso LPC1769 Emulator Not Found

3,084件の閲覧回数
yi_wang
Contributor I

hi all,

I am new here and just begin to work with the LPCXpresso LPC1769 eva-board for one demo project.

I installed LPCXpresso V8.22_650 IDE, LPC11Uxx-Debug-Probe-VCOM driver in my Win7 X64 system.

With the example programs I am able to compile, build, but not with debug or download to processor.

The error log is

"No compatible emulators available.
They may be disconnected, not powered, already in use or not compatible with this target".

However my eva-board is conneted without problem. I've tried all "shown Debugger" setting like "LPC-Link (WinUSB) or RDB-Link // LPC-Link (HID) //  Red Probe Family // Link Server", but nothing changed.

So can someone help me to solve this issue? Thanks so much.

Regards,

Yi

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,961件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, WangYi,

Do you use the keil board?

pastedImage_1.png

If you use the board, what is the debug device you are using? which connector are you using?

BR

Xiangjun Rong

0 件の賞賛
返信

2,961件の閲覧回数
yi_wang
Contributor I

Hello Xiangjun,

thanks for your reply.

No, I don't have the Keil LPC1769 you showed.

I have in hand the OM13085 eva board.

65656565.JPG

In principle I don't need any further HW component more.

BR,

Yi

0 件の賞賛
返信

2,960件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, WangYi,

I suggest you refer to the two figures, I use a board on which the  LPC11U35 CMSIS-DAP chip is embedded. On the device manager menu, the LPC11U35 is enumerated as LPC11U3x CMSIS-DAP device.

I use MCUXpresso IDE tools.

Hope it can help you

BR

Xiangjun Rong

pastedImage_3.png

pastedImage_2.png

0 件の賞賛
返信