LPCUSBLib for LPCOpen v2.04(LPC4330)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCUSBLib for LPCOpen v2.04(LPC4330)

1,701 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hayami on Thu Dec 19 19:38:33 MST 2013
Hi
Where i can download LPCUSBLib for LPCOpen v2.04(LPC4330) ??
i try to use old LPCUSBLib with LPCOpen v2.04(LPC4330), but it can't wrok :((
Thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,641 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sundarapandian on Mon Jan 27 13:58:53 MST 2014
LPCOpen v2.04 (http://www.lpcware.com/system/files/lpcopen_2_04_keil_iar_ngx_xplorer_4330.zip) has LPCUSBLib under "software" folder. The host example workspace for keil is at applications\lpc18xx_43xx\keil_uvision_projects\ngx_xplorer_4330\ngx_xplorer_4330_lpcusblib_host_examples.uvmpw, for IAR it is at applications\lpc18xx_43xx\iar_ewarm_projects\ngx_xplorer_4330\ngx_xplorer_4330_lpcusblib_host_examples.eww

LPCOpen does not support USB Device stack in LPCUSBLib. It is replaced with a better Device stack located in the ROM (see usbd_rom examples).
0 Kudos
Reply

1,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nmz787 on Sat Jan 18 17:20:42 MST 2014
I too want to know, I'm using an LPC4370 and am having the same difficulty getting up and running quickly.
0 Kudos
Reply