LPCUSB lpc1769 BulkIn ACK interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCUSB lpc1769 BulkIn ACK interrupts

1,228件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gnxp on Mon Feb 23 06:11:42 MST 2015
Hello,
I deleted a similar previous post after realising some gaps in my understanding. This post is to ask my query more clearly.
Environment - LPCUSB for lpc1769(from code RDB CMSIS)
After browsing some forum topics, I decided to use LPCUSB(Bertrik Sikken) as I found the code simple to follow.

I am failing here -
When I transfer more than 64 bytes on BulkIn, I expect to get a BulkIn Ack after transfer is completed.
Procedure is simple -
1. First 'NextBulkIn' call is from my firmware. I set BulkInBusy = true; Step 1 happens only if BulkInBusy is false.

2. Read data from buffer, send to EP. If data>64 bytes, BulkInBusy  stays true.
   I expect to get a BulkIn ACK interrupt. Read data from buffer again and send to EP. If data <64 this time or 0, set BulkIn to false.

3. This allows me to start from step1 again.

The issue is I don't get any BulkIn ACK interrupts.

###################################################

static void NextBulkIn(U8 bEP)
{
/** Read cnt from buff and do USBHwEPWrite **/

if (cnt < MAX_PACKET_SIZE)
     BulkInBusy = false;
}

static void BulkIn(U8 bEP, U8 bEPStatus)
{
if (bEPStatus & EP_STATUS_ERROR)
goto err;
if (bEPStatus & EP_STATUS_STALLED)
goto err;
if (bEPStatus & EP_STATUS_DATA)// No buffer empty
goto err;

NextBulkIn(bEP);
return;

err:
BulkInBusy = false;
}

#########################################################

First call to NextBulkIn is from firmware if BulkInBusy =false;

I am sure interrupts are enabled
##################################################
From Init func,
USBHwRegisterEPIntHandler(BULK_IN_EP, BulkIn);

which calls in LPCUSB

void USBHwRegisterEPIntHandler(U8 bEP, TFnEPIntHandler *pfnHandler)
{
int idx;

idx = EP2IDX(bEP);

ASSERT(idx<32);

/* add handler to list of EP handlers */
_apfnEPIntHandlers[idx / 2] = pfnHandler;

/* enable EP interrupt */
LPC_USB->USBEpIntEn |= (1 << idx);
LPC_USB->USBDevIntEn |= EP_SLOW;
}

From init function
USBHwNakIntEnable(0)

which calls in LPCUSB
void USBHwNakIntEnable(U8 bIntBits)
{
USBHwCmdWrite(CMD_DEV_SET_MODE, bIntBits);
}


############################################################################
So if I am setting cmd data to be 0 for DEV_SET_MODE, I think all ACK's should be enabled.

So if USBEpIntEn , USBDevIntEn and DEV_SET_MODE all are OK, any clues why am I still not receiving any BulkIn ACK interrupts.

ラベル(1)
  • USB

0 件の賞賛
返信
0 返答(返信)