LPCScrypt2.1 fails on LPC4370

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCScrypt2.1 fails on LPC4370

4,291件の閲覧回数
mj_brd
Contributor I

I want to boot LPC4370 using LPCscrypt. According to LPCScript_user_guide, firstly, MCU is configured to boot from USB0. Then, LPCScript is installed. Finally, when I ran boot_lpcscrypt script in the command prompt, "Nothing to Boot" is written on the command window!!.

I checked my board and its connections several times however, they were correct. Moreover, although I tested this method on both Linux and windows10, I face the same problem.

would you help me to solve this problem??

0 件の賞賛
返信
5 返答(返信)

4,279件の閲覧回数
converse
Senior Contributor V

Is this a custom board or a purchased board?

When you connect the board. what does Windows show in Device Manager? Have you installed the device driver?

0 件の賞賛
返信

4,269件の閲覧回数
mj_brd
Contributor I

Thank you for your kind reply.

Yes, this is a custom board. Photos of the Device manager, the Schematic, and the CMD prompt are attached. As shown in the photos, there are no new devices to be recognized in the device manager when the USB cable is connected to the computer!

Yes, LPCScrypt and device drivers are installed simultaneously and even separately.

 boot pins P2_9 and P1_2 set to L, P2_8 and P1_1 set to H.

0 件の賞賛
返信

4,262件の閲覧回数
converse
Senior Contributor V

So, to be clear, the problem is with your board, and not with LPCScrypt. You need to fix your board before you can do anything with LPCScrypt. Suggest you start with something simple, like trying to download and run an LED blinky *using a debugger*.

0 件の賞賛
返信

4,258件の閲覧回数
mj_brd
Contributor I

I have been working with LPC4370 for a couple of years and did several projects with that.!

The USB port of the schematic was only attached to the previous response. This board has been using to carry out the protection functions of digital relays and can be programmed by J-link perfectly. Now, I want to program it using LPCScrypt and USB0 but Windows and Linux can not recognize the USB port of LPC4370 which is the flash-less MCU.

how can I solve this problem?? I checked my board and it was OK!! 

I would be appreciated if you give me any viewpoints.

 

 

0 件の賞賛
返信

4,232件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello mj_brd,

How about the pin P2_7? Low it to have a try.

 

Regards,

Alice

0 件の賞賛
返信