LPCScrypt v1.8.2 for raspberry (arm)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCScrypt v1.8.2 for raspberry (arm)

1,855件の閲覧回数
vianneyfenart
Contributor II

Hello, i tried to use LPCScrypt v1.8.2 for upload my lpc43xx .bin file. It works perfectly with windows. but i want to use it with a linux raspberry distribution. The LPCScrypt v1.8.2 is only for x86 linux...there is possiblity to have arm distribution? thanks

0 件の賞賛
返信
2 返答(返信)

1,728件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, there are no plans to release a raspberry pi version of LPCScrypt.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

1,728件の閲覧回数
vianneyfenart
Contributor II

Is it a way to flash LPC43XX platform with a RASPBERRY in DFU mode ?

Is it possible with DFU-util????

Thanks

Le 23 mai 2018 à 14:03, lpcxpresso_support <[email protected]<mailto:[email protected]>> a écrit :

NXP Community<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPCScrypt v1.8.2 for raspberry (arm)

reply from LPCX support<https://community.nxp.com/people/lpcxpresso_support?et=watches.email.thread> in LPC - View the full discussion<https://community.nxp.com/message/1017108?commentID=1017108&et=watches.email.thread#comment-1017108>

0 件の賞賛
返信