LPCSPIFILib v0.04_beta available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCSPIFILib v0.04_beta available

1,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Mon Apr 28 21:11:36 MST 2014
LPCSPIFILib v0.04_beta available for download at http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages

[u]KEIL_IAR Package contains[/u]

1. Source for SPIFI Library (software/lpcspifilib/src)
2. Pre-compiled SPIFI Library (software/lpcspifilib/lib)
3. Library interface header files (software/lpcspifilib/inc)
4. Documentation/User Manual (software/lpcspifilib/docs)
5. LPCOpen example for Keil MCB 4357 board (applications/lpc18xx_43xx/{keil_uvision_projects|iar_ewarm_projects}/keil_mcb_4357/keil_mcb_4357_spifilib_examples.*)
6. Use the example with LPCOpen release version v2.09

[u]LPCXpresso Project[/u]

1. Example project (lpcspifilib)
2. Test suit project (spifilib_tst)
3. Pre-compiled library project (lib_lpcspifilib)
4. Import the project into the same workspace as LPCOpen v2.09 release for LPCXpresso
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,465件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by krhodesnb on Fri May 02 03:45:05 MST 2014
This is not a very usable page. The horizontal scroll bar only shows up at the very bottom of the entire page, which means I couldn't tell that column even existed.

Thanks.
0 件の賞賛
返信

1,465件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri May 02 03:18:58 MST 2014
It is there. Look in the "related downloads" column (which you may need to scroll left to see).
0 件の賞賛
返信

1,465件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by krhodesnb on Fri May 02 03:06:08 MST 2014
I don't see a file on the 43xx page with the SPIFI library source in it. Does it have proper permissions?
0 件の賞賛
返信