LPCOpen2.12 sdmmc / massstorage performance bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen2.12 sdmmc / massstorage performance bug

1,191 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mengxp on Sun Jun 12 23:01:19 MST 2016
void Chip_SDIF_SetClock(LPC_SDMMC_T *pSDMMC, uint32_t clk_rate, uint32_t speed)
{
/* compute SD/MMC clock dividers */
uint32_t div;

div = ((clk_rate / speed) + 2) >> 1;   <<< div here compute wrong

when I set speed=51MHz, div result is = 3.
so SD clock acturally be set at 204MHz / (2*3) = 34MHz.
SD bandwidth = 34M * 4 / 8 = 17MB/s
and test result is:

card_init
clk_rate: 204000000
speed: 20000000
div: 6
clk_rate: 204000000
speed: 51000000
div: 3
speed: 51000000
clk_rate: 0
Speed testing...
Read Speed: 14075 KB/s


I correct above bug code
div = (clk_rate / speed) >> 1;
so div will be set to 2 correctly, SD clock will be set at 204MHz / 2*2 = 51MHz
SD bandwidth = 51M * 4 / 8 = 25.5MB/s
and test result is

card_init
clk_rate: 204000000
speed: 20000000
div: 5
clk_rate: 204000000
speed: 51000000
div: 2
speed: 51000000
clk_rate: 0
Speed testing...
Read Speed: 19621 KB/s


see? that is a big improve!




And why the Mass Storoge example run at a bad performance about:
Read: 7MB/s
Bacause this example use a synchronous SD Read/Write
So read/write performance will be cut about a half.
Use double buffer and asynchronous SD read/write will do better performance
Labels (1)
2 Replies

1,145 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,145 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Mon Jun 13 08:42:00 MST 2016
Hi Mengxp,

Great work!  Thank you for tracking this down and providing your results!  We are reviewing your suggested fix across all clock ranges for updating the code base.  The issue and your fix have been logged in our internal LPCOpen system and will be fixed in our updates.

Best regards,
-NXP Support
0 Kudos
Reply