LPCOpen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen

1,805 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tridentsx on Thu Feb 14 10:43:59 MST 2013


Will LPCOpen support the LPC1347 MCU ? Will it support the embedded artists LPC expresso board for LPC1347 ?

Regards /// Carl
Labels (1)
0 Kudos
Reply
1 Reply

1,662 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Thu Feb 14 11:25:00 MST 2013
Hi Carl,

The next release (v1.01) should add support for the LPC1347 and the Xpresso 1347 board, but USB device/USB ROM support for that release isn't likely.
The driver API support will look very similar to the current 11xx CHIP driver API support (very similar peripherals).

That release is about 2 weeks away.
0 Kudos
Reply