LPCOpen v2.07 USB examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen v2.07 USB examples

1,254 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by YOZHik on Wed Feb 19 11:25:19 MST 2014
I downloaded LPCOpen v2.07 (IAR version) but can't find neither USB examples for LPC175x_6x devices nor any USB libraries included. Should I look anywhere else for an USB library to work with LPCOpen v2.07?
Labels (1)
0 Kudos
Reply
1 Reply

1,226 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Feb 19 11:35:34 MST 2014
See #6 of:

http://www.lpcware.com/content/forum/post-lpcopen-feedback-here


Quote:
The USBDLIB and USBDROM examples didn't make it into this release. They are planned for an upcoming release along with some additional examples, improvements, and fixes for known issues. (See http://www.lpcware.com/content/project/lpcopen-software-development-platform-nxp-lpc-microcontroller...)

So when is the date for the upcoming release? It could be as little as 2 weeks and as long as 6. Sad
However - if we can - we'll try to provide some early code for usbd_lib/usbd_rom prior to that release.

Kevin Wells

NXP Semiconductors

0 Kudos
Reply