LPCOpen on LPC1788 with 7 inch LCD (embedded artists)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen on LPC1788 with 7 inch LCD (embedded artists)?

1,154件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by skaara on Fri Aug 09 04:06:46 MST 2013
Hi,
I am quite new to ARM programming and this problem might be very easy to solve, but I'm really struggling here: I want to use the 7" LCD from embedded artists on the LPC1788 devkit (also embedded artists) with the LPCOpen platform (v1.03), but I don't know how to initialize it using the LPCopen functions --  does anyone know of or have an example that shows how to do it? The examples that are included with LPCOpen only show how to use the 3.2" LCD which is connected via the QVGA display adapter.
Any help would be highly appreciated!
Thanks,
Gregor
ラベル(1)
0 件の賞賛
返信
1 返信

1,084件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Aug 09 06:54:07 MST 2013
Hi,
I suggest you to use following BSP first. It works on EA board with 7 inch LCD without any problem. Based on this you can perform changes in LPC open example code for 7 inch LCD.

http://www.lpcware.com/content/nxpfile/emwin-520-board-support-package-ea1788-board
0 件の賞賛
返信