LPCOpen for LPCxpresso 1769: where is the debug uart port?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen for LPCxpresso 1769: where is the debug uart port?

1,336 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Thu Apr 16 02:25:45 MST 2015
lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip comes with an example of UART peripheral. In README.txt I read:

Special connection requirements
[...]
- LPCXpresso LPC1769:
Need to connect with base board for using RS232/UART port.


I can't understand. Where is the UART port used in the examle? I see the port is UART3, but where is it? Is there a virtual serial port on USB connection to LPC-Link?
标签 (1)
0 项奖励
回复
4 回复数

1,285 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Thu Apr 16 06:15:58 MST 2015
Ok, now I understand. I didn't knew the baseboard product  ;-)
0 项奖励
回复

1,285 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Apr 16 05:43:11 MST 2015
No. Try searching for "LPCXpresso Baseboard"
0 项奖励
回复

1,285 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Thu Apr 16 03:51:43 MST 2015
What is "base board"? Is it the LPCxpresso board? If yes, what are the RX/TX pins to use?
0 项奖励
回复

1,285 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Apr 16 03:49:51 MST 2015
Whats not clear?

Quote:
Need to connect with base board for using RS232/UART port.


Can that be any clearer?
0 项奖励
回复