LPCOpen for LPC1759

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen for LPC1759

2,001件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by osanchez on Mon Jan 26 02:07:04 MST 2015
Hi,

I'm starting developing for the LPC1759.

As I can see, LPCOpen is recommended instead of CMSIS-CORE. So, I stopped working with CMSIS and want to use LPCOpen.

However, in the downloading page, I only see support for LPC17xx in version 1.xx.

Is this an stable version? Is it save to start developing using v1.03?

Regards,

Oscar
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,985件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Jan 26 05:41:04 MST 2015

Quote: osanchez
I'm not interested in developing for a specific board.



:D

LPCOpen is using this board library to make a few things easier...

http://www.lpcware.com/content/faq/how-do-i-port-lpcopen-new-baord

If you start with a new project (which has hopefully a board  :) ) just make a copy of the LPCXpresso board library and use this copy. Of course you can also work without board library and use CMSIS core only.

I'm not sure what you are trying to do and if you want to use samples  :)

In general it's useful to understand this board library and with a few changes (LEDs, IOCON settings...) your non-board LPC1759 is working with LPCOpen samples...

0 件の賞賛
返信

1,985件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by osanchez on Mon Jan 26 05:24:50 MST 2015
Thank you for the answer.

I'm not interested in developing for a specific board. As I can see, the latest version V2.10 is for two specific boards, and none of them includes the LPC1759.

Is it possible to download version V2.10 and still compile for LPC1759?

Is there any example that targets a given processor but not a specific board?
0 件の賞賛
返信

1,985件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jan 26 02:12:14 MST 2015
The latest version is v2.10 and can be downloaded from here:
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages

The latest versions of all LPCOpen packages can be found here:
http://www.lpcware.com/content/nxpfile/lpcopen-platform
0 件の賞賛
返信