LPCOpen for LPC13xx doesn't seem to contain USB examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen for LPC13xx doesn't seem to contain USB examples

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by prowley on Thu Mar 20 20:35:53 MST 2014
Hi,
Trying to start up a LPC1343 using USB, and the LPCOpen 2.05 download doesn't seem to contain the USB libraries, or a workspace/project for the USB examples.  Am I missing something?

Also, I downloaded v1.03, and it compiles fine for LPC1347, but is missing the BSP for the 1343.

Where could I get the board files for v1.03, or the USB examples/library for 2.05?

Thanks
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,609件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dmasyukov on Thu Dec 11 14:14:01 MST 2014

Quote: prowley
I see examples for the LPC1347, but nothing for the LPC1343.  From my understanding the USB implementations are not the same between the two parts.



For the examply the same reason I had to create an example myself. This project uses USB peripheral directly and therefore it's possible to create any USB device - https://bitbucket.org/dmasyukov/justhidusb
0 件の賞賛
返信

2,609件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dmasyukov on Thu Dec 11 14:12:20 MST 2014

Quote: embd02161991
Hi ,

You can find USB example projects form the following links :

http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc1311134243-peripherals-using-keils-mdk-...

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc13xx-packages

Download the LPCXpresso version of LPCOpen v.2.05  for LPC1343 and you will find USB examples there.



Thanks,

NXP Technical Support



No, there are none! I've looked really hard.
0 件の賞賛
返信

2,609件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by twols on Mon Sep 15 07:48:59 MST 2014
The same problem here. The examples only work for LPC1347... Not for 1343!!
0 件の賞賛
返信

2,609件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by prowley on Fri Mar 21 13:34:36 MST 2014
I see examples for the LPC1347, but nothing for the LPC1343.  From my understanding the USB implementations are not the same between the two parts.
0 件の賞賛
返信

2,609件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Mar 20 21:37:34 MST 2014
Hi ,

You can find USB example projects form the following links :

http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc1311134243-peripherals-using-keils-mdk-...

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc13xx-packages

Download the LPCXpresso version of LPCOpen v.2.05  for LPC1343 and you will find USB examples there.



Thanks,

NXP Technical Support
0 件の賞賛
返信