LPCOpen code for lpc54100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen code for lpc54100

1,217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ocind on Thu Mar 26 01:53:25 MST 2015
Hi all,

I was experimenting with the rom_spim_int sample code of LPC54100 microprocessor. I am using LPCXpresso IDE and OM13077 demo board for my LPC54100.

If I changed the CPHA&CPOL mode into 1 or 3, I find this issue that whenever I modified the number of items sent in a SPI transfer to a value less than 3 (constant BUFFSENDSIZE in the sample code), the code would simply get stuck in the transfer handle. Is this a known issue with the LPCOpen sample code for this microprocessor?

Attached code gets stuck when it is run on the OM13077.

Thank you.

Original Attachment has been moved to: code.c.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,163 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nicolasdarmadja on Sun Apr 05 10:20:46 MST 2015
Similar issue here.. Have you found the solution yet?
0 Kudos
Reply