LPCOpen code for lpc54100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen code for lpc54100

1,200件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ocind on Thu Mar 26 01:53:25 MST 2015
Hi all,

I was experimenting with the rom_spim_int sample code of LPC54100 microprocessor. I am using LPCXpresso IDE and OM13077 demo board for my LPC54100.

If I changed the CPHA&CPOL mode into 1 or 3, I find this issue that whenever I modified the number of items sent in a SPI transfer to a value less than 3 (constant BUFFSENDSIZE in the sample code), the code would simply get stuck in the transfer handle. Is this a known issue with the LPCOpen sample code for this microprocessor?

Attached code gets stuck when it is run on the OM13077.

Thank you.

Original Attachment has been moved to: code.c.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,146件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nicolasdarmadja on Sun Apr 05 10:20:46 MST 2015
Similar issue here.. Have you found the solution yet?
0 件の賞賛
返信