LPCOpen and RS485 with address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen and RS485 with address

1,658件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tschnagel on Thu Oct 09 12:53:17 MST 2014
Hello All,
  Does anybody have any sample code using LPCOpen v2 with RS485 multi-drop using the address?  I've gotten this to work with CMSIS but I can't seem to get my head around trying to do this on LPCOpen.

I'm using LPC1115 (acutally LPCXpresso board for testing).  Also using LPCXpresso v7.3.0

Any help would be appreciated.

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 返信

1,589件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thommaughan on Thu Nov 06 21:20:57 MST 2014
I'm also interested if there are plans to release something like what I see with LPCopen 1.03... 

I'm just starting to look at what it will take to manage the 'detect end of last byte transmission' in order to de-assert the rs485 tx_enable...   I'm presently polling the transmit ring buffer empty condition and then waiting for a timed delay for the byte to transfer - not the best way, but it's a start.
0 件の賞賛
返信