LPCOpen USB CDC sample not work with my LPC1549 custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen USB CDC sample not work with my LPC1549 custom board

2,478 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hardtail on Mon Mar 02 07:38:00 MST 2015
HI, guys

I made custom board with LPC1549. the USB-ISP works as expected in this hardware.However, when the USB-CDC sample run, Windows doesn't recognize it.

I added LED blink code using  SysTick to this sample, and I make sure runing this code. So LPC1549 was not hang.

I tried sample of USBDevice for Mbed. it code run without problem. so i think that hardware doesn'd have problem.

Does anyone have any ideas on what I can try?



标签 (1)
0 项奖励
回复
4 回复数

2,383 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hardtail on Tue Mar 03 07:49:06 MST 2015
Thank you for your answer R2D2 again.

I rewrote code about  PIO0_16 as VBUS in board_sysinit.c. Then it work as expected!

I solved the problem with your advice.

many thanks!!
0 项奖励
回复

2,383 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Mar 03 02:18:44 MST 2015

Quote: hardtail
This image is a part of my hardware's schema.



ISP Pins?

Which sample are you using in detail? Which board layer (http://www.lpcware.com/content/faq/how-do-i-port-lpcopen-new-baord)?

What's showing your Device Manager? Which Windows are we talking about?

CDC is working fine here with Win7 / Win8 and Win10  :O

Note: LQFP48 is using PIO0_16 instead PIO1_11 as VBUS, so a wrong Pin muxing in board_sysinit.c will keep your USB from working  :p
0 项奖励
回复

2,383 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hardtail on Tue Mar 03 01:08:07 MST 2015
Thank you for your fast answer R2D2.

This image is a part of my hardware's schema. My hardware is not connect  RTCXOUT, RTCXIN and VBAT. That is Major difference between  LPC1549 LPCXpresso Board and my hardware. but I think that peripheral RTC has nothing to do with USB-CDC.
[img]http://i.gyazo.com/5ed64eb3468d24caa55e75b6c33a6dcb.png[/img]
0 项奖励
回复

2,383 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Mar 02 11:09:09 MST 2015

Quote: hardtail
Does anyone have any ideas on what I can try?



Compare your hardware with LPC1549 LPCXpresso Board  :)
0 项奖励
回复