LPCOpen Platform for LPC11XX microcontrollers v2.00a applied on LPC11U35

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen Platform for LPC11XX microcontrollers v2.00a applied on LPC11U35

1,158 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by liaochengyi on Fri Oct 11 11:22:15 MST 2013
I download LPCOpen Platform for LPC11XX microcontrollers v2.00a
The document wrote:

"Supported boards and board setup:

NXP LPCXpresso LPC11U14 board
NGX Blueboard LPC11U24 board
NXP LPCXpresso LPC11C24 board
Mcore48 LPC1125 board"

I tried use "freertos blinky example code" apply to LPC11U35 chip, but can't work.
The debug stop at HardFault_Handler()

Is the LPCOpen Platform code base need to modify for LPC11U35 chip?

Thank you for your answer!!
标签 (1)
0 项奖励
回复
1 回复

1,118 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by liaochengyi on Sat Oct 12 04:33:03 MST 2013
I given up use the LPCOpen Platform code base for LPC11U35,
then create new project and include the necessary library.

It's works now.

I think the LPCOpen Platform code base (LPC1114) can not apply to LPC11U35 directly.
(The basic memory setting has different and need effort to modify.) 
0 项奖励
回复