LPCOpen LPC18xx Missing things

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen LPC18xx Missing things

1,378 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brunoalmeida on Thu Jul 24 18:28:51 MST 2014
Hi There,

  The LPCOpen for NGX Xplorer LPC1830 board (lpcopen_2_12_lpcxpresso_ngx_1830) is missing some files for the LPCUSBLib Project. Files like device.h and device.c are important for USBController to build for example. 
Labels (1)
0 Kudos
Reply
2 Replies

1,364 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brunoalmeida on Fri Jul 25 15:16:37 MST 2014
Hi there,

I did not notice that the project was Host only... and not HostDevice like the sample code from OM13061, and maybe i had the flag USB_CAN_BE_DEVICE set. Thanks for the help.
0 Kudos
Reply

1,364 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 25 00:23:00 MST 2014
I see no  build problems with the lpcusblib_MassStorageHost, lpcusblib_KeyboardHost or lpcusblib_AudioOutputHost projects from this package.

Can you clarify exactly what problems you are seeing? What version of LPCXpresso are you using? Can you post your build log?

http://www.lpcware.com/content/faq/lpcxpresso/build-console

Regards,
LPCXpresso Support
0 Kudos
Reply