LPCOpen I2C example project slave mode not working: cannot probe or read.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen I2C example project slave mode not working: cannot probe or read.

903件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lerlacher on Sun Apr 13 08:41:01 MST 2014
I am using the LPCOpen I2C example with an LPC11C24 breakaway board, programmed with LPC-Link.

I just compiled and uploaded the image (with LPC-Link), and it runs, but I can't probe or read the two simulated slave devices.
I am doing the probing and reading from a raspberry pi using the linux i2c-tools.
I'm pretty sure the raspberry pi and the bus are set up correctly. To make sure, I also have an arduino running as a slave on the same bus, and I can probe and read it without problems.

Sadly I don't have a base board here so I don't have a UART connection to use the menu in the example, but the code looks like the slaves should be working despite that.

Is there anything obvious or any errata in the example code that I'm missing?

Best,
Luke
ラベル(1)
0 件の賞賛
返信
0 返答(返信)