LPCOpen FreeRTOS 10.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen FreeRTOS 10.0?

1,411件の閲覧回数
danielholala
Senior Contributor II

Dear NXP,

I imported and compiled the freertos_blinky exampled which is included in "lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769". It contains FreeRTOS 8.0.1 port. 

Is there any plan to update LPCOpen drivers/examples/libraries to the recent FreeRTOS version 10.0?

For the time being, I'm using the original source code downloaded by freertos.org.

Cheers,

Daniel

0 件の賞賛
返信
1 返信

1,277件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi danielholala,

    Unfortunately, until now, I didn't get any information about that lpcopen updation.

   So, if you want to get the updated example with the latest FreeRTOS, I think, you need to import it by yourself.

 

   Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信