LPCLink2 is unable to recognize lpc812 cortex m0 mcu by SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCLink2 is unable to recognize lpc812 cortex m0 mcu by SWD

1,475件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dizgah on Sun Apr 24 00:22:28 MST 2016
I'm trying to debug a simple blinky program via lpclink & lpcxpresso to lpc812 mcu,lpc812 is mounted on very simple header board which pinned out it's GPIOs.I can successfully program and run mcu with Flashmagic,Also with Jlink and keil i can debug program to the mcu's SRAM memory,but it cant debug programs on FLash memory too.LPCXpresso can connect to LPCLINK and recognized it successfully but cant detect mcu.
[img]http://i.stack.imgur.com/Ux7zP.gif[/img]
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,423件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,423件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by schoeler on Wed Apr 27 09:33:59 MST 2016
Verify that the ISP mode entry pin (PIO0_12) is held high
0 件の賞賛
返信

1,423件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 25 07:43:03 MST 2016
In the first place, check out:

https://www.lpcware.com/content/faq/lpcxpresso/debug-design

Regards,
LPCXpresso Support
0 件の賞賛
返信