LPCLink-2 (As Evaluation Board) Double Powered?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCLink-2 (As Evaluation Board) Double Powered?

1,195件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Mar 13 23:06:32 MST 2015
What happens when a LPCLink-2 board is powered both by the probe (probe has J2 closed) AND by
USB (target is connected to PC). Will I damage the target LPCLink-2?

How does this affect resetting. Via debug launch, via plug/unplug (target) USB cable.

Regards, Mike.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,189件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Mar 16 17:17:28 MST 2015
Thank you very very much for that.

That is what I was hoping for, but I am a software guy not a hardware expert.

The reason: I would like to 'reset' the target and re-download edited code via dfu,
but it is always nice not to have to 'loose' the debugger on the other board.

Regards, Mike
0 件の賞賛
返信

1,189件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Mon Mar 16 04:17:52 MST 2015
That connects the outputs of the 3.3V regulators on the two boards. But since the XC6227 regulator has reverse current protection that shouldn't be a problem (no guarantees, please check schematics and data sheet for yourself).

Basically the target board will be powered when at least one of the power sources is available.
0 件の賞賛
返信