LPCExpresso LPC812 Rev B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCExpresso LPC812 Rev B

1,630件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Fri Sep 27 09:48:48 MST 2013
I can only find the schematic for Rev A.
checked EA web site, checked www.lpcware web site
I assume the only difference is the ISP pin was moved with Rev 4C parts.
Nice part NXP!
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,564件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpecosystem on Tue Oct 21 08:00:17 MST 2014
The Rev A schematics are here:
http://www.lpcware.com/system/files/LPCXpresso%20LPC800%20rev%20A.pdf

Sorry you had this trouble - the links to the schematics should be on the nxp.com site, and we will get that corrected.
0 件の賞賛
返信

1,564件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Sat Oct 18 12:04:58 MST 2014
Where do I find the schematic for LPC812 LPCXpresso rev. A schematic? Although I could figure out what it looks like based on the previous post, I prefer to have the schematic to reflect the board I have.

Why is it so difficult to find the schematics for LPC812 LPCXpresso? I would expect to find a link to all relevant documentation on the "home page" of the board which appears at http://www.nxp.com/demoboard/OM13053.html. This page is a bit thin: Documentation tab holds no documents!
0 件の賞賛
返信

1,564件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Mon Sep 30 11:16:09 MST 2013
Thank you for bringing this to our attention.
The LPC812 LPCXpresso rev B schematics have been uploaded to LPCWare.  You can download the schematics from:
http://www.lpcware.com/content/nxpfile/lpcxpresso-board-schematics-lpc800-rev-b
The only difference I could see was moving PIO0_12 to pin 8 of the UART header compared with rev A which had PIO0_1 going to pin 8 of the UART header.  As you already mentioned, this change was required due to the moving of the ISP pin from PIO0_1 to PIO0_12.
0 件の賞賛
返信