LPCD Mode CLRC663

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCD Mode CLRC663

2,582 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPCconvadis on Thu Feb 05 01:01:30 MST 2015
Hi,

I'm sorry if I'm writting on the false forum, but I don't know where can I put my question.

I'm trying to use the LPCD mode with the RFID IC CLRC663 whitout success. I'm using the following functions from the NXP library:
- phhalHw_Rc663_Cmd_Lpcd
- phhalHw_Rc663_Cmd_LpcdConfig

At the first time I configure the CLRC663 with the function "phhalHw_Rc663_Cmd_Lpcd" and then I get the values for I and Q. Then I put these values into the next function but the IC does not generate any interrupt when I put a card near the feld.

Is there any example how I have to configure these funcionts and the IC? Or maybe some hints?

I'd appreciate for any help.

Thank you in advance.

Pablo
标签 (1)
0 项奖励
回复
1 回复

2,174 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 05 02:43:04 MST 2015
Sorry, the NFC guys don't hang out here. But you can find CLRC663 related information at:

http://www.nxp.com/products/identification_and_security/nfc_and_reader_ics/nfc_contactless_reader_ic...

Click on the 'Design Support' tab for assistance

Regards,
LPCXpresso Support
0 项奖励
回复