LPCD Mode CLRC663

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCD Mode CLRC663

2,526件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPCconvadis on Thu Feb 05 01:01:30 MST 2015
Hi,

I'm sorry if I'm writting on the false forum, but I don't know where can I put my question.

I'm trying to use the LPCD mode with the RFID IC CLRC663 whitout success. I'm using the following functions from the NXP library:
- phhalHw_Rc663_Cmd_Lpcd
- phhalHw_Rc663_Cmd_LpcdConfig

At the first time I configure the CLRC663 with the function "phhalHw_Rc663_Cmd_Lpcd" and then I get the values for I and Q. Then I put these values into the next function but the IC does not generate any interrupt when I put a card near the feld.

Is there any example how I have to configure these funcionts and the IC? Or maybe some hints?

I'd appreciate for any help.

Thank you in advance.

Pablo
ラベル(1)
0 件の賞賛
返信
1 返信

2,118件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 05 02:43:04 MST 2015
Sorry, the NFC guys don't hang out here. But you can find CLRC663 related information at:

http://www.nxp.com/products/identification_and_security/nfc_and_reader_ics/nfc_contactless_reader_ic...

Click on the 'Design Support' tab for assistance

Regards,
LPCXpresso Support
0 件の賞賛
返信