LPC8N04 can't start without debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC8N04 can't start without debugger

1,305 Views
ertqwert
Contributor I

Hi, sorry for the translator

My LPC8N04 can't start without debugger. 

I've seen threads

LPC8N04 Boot ROM Change 0.12 to 0.14 and 

Can't build LPC8N04 / OM40002 example code in "release" mode but it didn't help.

I tried writing 0 instead of the checksum, it also did not help

Chip time stamp 743

Boot code 0x1A000C - use IAP api

I use a custom board

Labels (1)
0 Kudos
Reply
1 Reply

1,262 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Nik

This is LPC8N04 boot ROM checksum issue.  Please check this article. hope this will help you.

[LPC8N04]LPC Boot ROM checksum 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply