LPC865 ram issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC865 ram issue

1,301 Views
TeemoLi
Contributor III

The part number LPC845M301JHI48K.

VDD ~ 1.3Voltage.  It can works。

Sometimes it gets erased.  Which memory voltage will cause the Flash to be erased.

Or does undervoltage not change or erase data?

Is the normal Flash operating voltage 1.8V or how many voltage ?

 

 

0 Kudos
Reply
1 Reply

1,282 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @TeemoLi 

I hope that you are doing well! 

According to the LPC845 Datasheet, the minimum voltage for VDD is 1.8v.

diego_charles_0-1700165283987.png

The normal operating voltage is 3.3v. 

As a general reply, if the voltage is below the specification there is no guaratee for the MCU to behave properly. 

The LPC845 integrates an brownout protection mechanism, which maintains the device in a reset if the VDD voltage falls below the expected. Because if the VDD specifications are not meet, the device may malfunction. 

This a general reply from my side. If you have more concerns about this or more details, like the test situation or scenario that you are facing to get 1.3v, do not hesitate to let me know. 

All the best, 

Diego

 

 

0 Kudos
Reply