LPC865 UART0 polling receiver problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC865 UART0 polling receiver problem.

1,344 Views
Berlin
Contributor I

 

Hi NXP,

I'm using the LPC865M201JHI48 microcontroller for UART communication. The transmit function works correctly (I verified this using a serial terminal like PuTTY), but the receive function is not working properly.

What I'm working on:
I'm trying to interface the ESP8266 Wi-Fi module with my LPC865M201JHI48 controller. When I send the "AT" command to the Wi-Fi module over UART, I expect to receive an "OK" response from the module. However, instead of receiving "OK", I'm continuously getting the character 'A'.

Note:
The ESP8266's blue LED is blinking during this process, which indicates that the module is transmitting data (TX activity). This confirms that the ESP8266 is responding, but my microcontroller is not receiving the data correctly.

pin connection

ESP8266 Pin Connect to LPC865

VCC3.3V
GNDGND
TXRX of LPC (UART0_RX - PIO0_31)
RXTX of LPC (UART0_TX - PIO1_9)
CH_PD (EN)Pull HIGH (3.3V)
RSTPull HIGH (3.3V)

char response[128];

 

/*void UART0_SendChar(char c) {

while (!(USART0->STAT & (1 << 2)));

USART0->TXDAT = c;

}

void UART0_SendString(const char *str) {

while (*str) UART0_SendChar(*str++);

}

 

void send_AT(const char *cmd, uint32_t delay_time) {

UART0_SendString(cmd);

// UART0_SendString("\r\n");

delay_ms(delay_time);

}

 

void UART0_ReceiveFullResponse(char *response, int max_len)

{

int i = 0;

char c;

uint32_t timeout;

int newline_count = 0;

 

while (i < (max_len - 1))

{

timeout = 200000;

 

while (!(USART0->STAT & USART_STAT_RXRDY_MASK) && --timeout);

if (timeout == 0) break;

 

c = USART0->RXDAT;

response[i++] = c;

 

// Optional: Count newlines to wait for complete response

if (c == '\n' || c == '\r') {

newline_count++;

if (newline_count >= 2) break; // Assume full response after 2 line breaks

}

}

 

response[i] = '\0';

}

 

 

 

char LPUART0_receive_char(void)

{ /* Function to Receive single Char */

char receive;

while((USART0 ->STAT & USART_STAT_RXRDY_MASK)>>USART_STAT_RXRDY_SHIFT==0);

/* Wait for received buffer to be full */

receive= USART0->RXDAT; /* Read received data*/

return receive;

}

 

// === MAIN ===

int main(void)

{

usart_config_t config;

// === Init ===

BOARD_InitBootPins();

BOARD_InitBootClocks();

BOARD_InitBootPeripherals();

CLOCK_Select(kUART0_Clk_From_MainClk);

USART_GetDefaultConfig(&config);

 

config.enableRx = true;

config.enableTx = true;

config.baudRate_Bps = BOARD_DEBUG_USART_BAUDRATE;

 

// USART_Init(USART0, &config, CLOCK_GetFreq(kCLOCK_MainClk));

USART_Init(EXAMPLE_USART, &config, EXAMPLE_USART_CLK_FREQ);

delay_ms(2000);

// Init system modules

main_init();

init_key();

spi_init();

tft_init();

//wifi pins

GPIO->DIR[0] |=(1<<24); // PIO0_24-->Enable

GPIO->DIR[0] |=(1<<13); // PIO0_13-->Reset

 

GPIO->SET[0] |=(1<<24); //En set

// To reset ESP8266

GPIO->CLR[0] |= (1 << 13); // Assume PIO0_13 connected to RST

delay_ms(100); // Hold low

GPIO->SET[0] |= (1 << 13); // Pull high again

 

 

fan_off();

buzzer_off();

boot_screen();

heater_off();

 

idel_mode_flag = ON;

current_mode = 0;

boot_done_flag = 1;

 

while (1)

{

send_AT("AT\n\r", 1000); // Send command

UART0_ReceiveFullResponse(response, sizeof(response));

displayText12x8(10, 10, response, YELLOW_COLOR, BLACK_COLOR); // Or print to UART for debugging

delay_ms(500);

display_clr(BLACK_COLOR);

delay_ms(500);

}

}*/

Baud rate : 115200

Could you please help me identify and resolve this issue?

Thank you

Labels (1)
0 Kudos
Reply
2 Replies

1,316 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Berlin 

Based on the information you provided,

You configured LPC865 UART for 115200 baud, but is the clock source precise enough? And does the ESP8266 expect exactly 115200?

I think you can capture the transmitted waveform and received waveform under the oscilloscope.

If the waveform is correct, you can then debug the code logic.

BR

Harry

0 Kudos
Reply

1,104 Views
Berlin
Contributor I

Okay… just leave that. In UART polling method, I’m able to send data from the microcontroller to the UART0 terminal, and it works well. However, when I try to receive data, it doesn’t work. Can you give me an example code for receiving data?

0 Kudos
Reply